Appendix A - wireless security - Johnson Controls - LIT-12013765 - Wireless field bus - Smart Equipment Control

Smart Equipment Control Wireless Installation Guide

Product
Controls > Smart Equipment Controls > Smart Equipment Control
Document number
LIT-12013765
Revision date
2021-02-17
Product status
Active

The WRG1830/ZFR183x Pro Series Wireless Field Bus System is secure for the following reasons:

  • The ZFR183x mesh over-the-air communication uses AES128 bit security.
  • The ZFR183x mesh network coordinator manages when devices can be added to the network and is able to be software locked to prevent unauthorized access.
  • The WRG1830 Gateway uses secure boot upon initialization and connection to the Ethernet network.
  • The ZFR183x Pro Series Wireless Field Bus devices transmit data using several short proprietary messages that are collected and reconstructed at the destination. If a piece of the message is intercepted, it is indecipherable to the outside source.
  • The WRG1830 Gateway requires authentication for user access with an audit log to track log-ins and commands.
  • The WRG1830 Gateway Wi-Fi functionality allows access to the wireless network configuration, but it does not create a Wi-Fi hotspot to the Internet.