Features - Johnson Controls - LIT-1921695 - T-4100 - Pneumatic Thermostat - Room Thermostat - Single Temperature Low Volume Output Thermostat

Single Temperature Low Volume Output Thermostat Catalog Page

Product name
Single Temperature Low Volume Output Thermostat
Document type
Catalog Page
Document number
LIT-1921695
Revision date
2020-01-10
  • mounts vertically
  • provided with exposed or concealed set point adjustment
  • available as Direct Acting (DIR) orReverse Acting (REV) model
  • includes standard Fahrenheit and Celsius thermometer
  • requires only one air connection with the use of a remote restrictor
  • available in vertical only