To Order - Johnson Controls - LIT-1900205 - RT-2000 Combination Fire and Smoke Damper

RT-2000 Combination Fire/Smoke Damper Catalog Page

Product
Dampers > Fire and Smoke Dampers > RT-2000 Combination Fire and Smoke Damper
Document number
LIT-1900205
Revision date
2021-03-10

Specify the code number from the selection chart. RT-2000 fire/smoke dampers are available in one inch increments. Actual damper size is 1/4 inch less than nominal. All Johnson Controls® damper dimensions are from the outside-edges of the damper frame.

All Johnson Controls Dampers are built to order, just in time, and cannot be returned due to customer ordering errors. All dampers are backed by a three-year warranty, which covers defects in materials or workmanship when used in our defined applications. Refer to terms and conditions of sale for specifics.