Standard objects - Johnson Controls - LIT-12014365 - RA-1270 - Airflow Measuring Station - RA-1270 Fan Inlet Airflow and Temperature Measurement Station
RA-1270 Protocol Implementation Conformance Statement
Product
Controls > Temperature Controls > RA-1270 Fan Inlet Airflow and Temperature Measurement Station
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12014365
Revision date
06/02/2024
Product status
Active
The device supports the following standard object types:
Device
Analog value
Notification class