Related documentation - Johnson Controls - LIT-12014420 - RA-1270 - Airflow Measuring Station - RA-1270 Fan Inlet Airflow and Temperature Measurement Station

RA-1270 Fan Inlet Airflow and Temperature Measurement Station SA Bus Integration Application Note

Product
Controls > Temperature Controls > RA-1270 Fan Inlet Airflow and Temperature Measurement Station
Document type
Application Note
Document number
LIT-12014420
Revision date
17/05/2024

For additional information on Equipment Controllers, see the following table:

Table 1. Related documentation
For information about: Refer to:
Programming and Commissioning Metasys Equipment Controllers Controller Tool Help (LIT-12011147)
CCT and Equipment Controller Package Licensing Software Manager Help (LIT-12012389)
MS/TP Communication, SA Bus rules and specifications MS/TP Communications Bus Technical Bulletin (LIT-12011034)