Introduction - Johnson Controls - LIT-12014420 - RA-1270 - Airflow Measuring Station - RA-1270 Fan Inlet Airflow and Temperature Measurement Station

RA-1270 Fan Inlet Airflow and Temperature Measurement Station SA Bus Integration Application Note

Product
Controls > Temperature Controls > RA-1270 Fan Inlet Airflow and Temperature Measurement Station
Document type
Application Note
Document number
LIT-12014420
Revision date
17/05/2024

The Johnson Controls® RA-1270 is an advanced electronic thermal dispersion fan and inlet air measurement device that reports airflow and air temperature.

Use the information in this document to connect and configure the RA-1270 with the Equipment Controller Generic SA Bus (GSAB).

Figure 1. RA-1270 Fan Inlet Airflow