Output data points as application inputs - Johnson Controls - LIT-12014420 - RA-1270 - Airflow Measuring Station - RA-1270 Fan Inlet Airflow and Temperature Measurement Station

RA-1270 Fan Inlet Airflow and Temperature Measurement Station SA Bus Integration Application Note

Product
Controls > Temperature Controls > RA-1270 Fan Inlet Airflow and Temperature Measurement Station
Document type
Application Note
Document number
LIT-12014420
Revision date
17/05/2024

You can add Read/Write output data points to Miscellaneous inputs with the EasyCAF tool. This duplicates output points on the input side in the CCT to use for the application. See the following figures.

Figure 1. Adding data points to Miscellaneous inputs in EasyCAF
Figure 2. Miscellaneous inputs in the CCT