Adding GSAB devices using the CCT - Johnson Controls - LIT-12014420 - RA-1270 - Airflow Measuring Station - RA-1270 Fan Inlet Airflow and Temperature Measurement Station

RA-1270 Fan Inlet Airflow and Temperature Measurement Station SA Bus Integration Application Note

Product
Controls > Temperature Controls > RA-1270 Fan Inlet Airflow and Temperature Measurement Station
Document number
LIT-12014420
Revision date
2024-05-17

When you use the CCT to add GSAB devices, the dialog window includes the following options:

  • Application selection. When applications are available, it is mandatory to select one of them. This provides all the data points that belong to the application.
  • Data points selection. Some points are dependencies of other points. If you select a point with dependency, you cannot select its dependent points. See Point mapping for more information.
  • Optional: Point name prefix modification.
Figure 1. Add Device dialog window in the CCT