When you use the CCT to add GSAB devices, the dialog window includes the following options:
- Application selection. When applications are available, it is mandatory to select one of them. This provides all the data points that belong to the application.
- Data points selection. Some points are dependencies of other points. If you select a point with dependency, you cannot select its dependent points. See Point mapping for more information.
- Optional: Point name prefix modification.
Figure 1. Add Device dialog window in the CCT