Vendor component requirements - Johnson Controls - LIT-12014420 - RA-1270 - Airflow Measuring Station - RA-1270 Fan Inlet Airflow and Temperature Measurement Station

RA-1270 Fan Inlet Airflow and Temperature Measurement Station SA Bus Integration Application Note

Product
Controls > Temperature Controls > RA-1270 Fan Inlet Airflow and Temperature Measurement Station
Document type
Application Note
Document number
LIT-12014420
Revision date
17/05/2024

The GSAB integration for Johnson Controls Equipment Controllers and the Johnson Controls RA-1270 is for the equipment shown in the following table.

Table 1. Vendor components and documentation
Device type Description
RA-1270 Fan inlet airflow and temperature measurement station
Documentation RA-1270 Protocol Implementation Conformance Statement (LIT-12014365)