Navigating the start-up menu - Johnson Controls - LIT-12014081 - RA-1270 - Airflow Measuring Station - RA-1270 Advanced Thermal Dispersion Fan Inlet Airflow and Temperature Measuring System

RA-1270 Advanced Thermal Dispersion Fan Inlet Airflow and Temperature Measuring System Technical Bulletin

Product
Controls > Temperature Controls > RA-1270 Advanced Thermal Dispersion Fan Inlet Airflow and Temperature Measuring System
Document number
LIT-12014081
Revision date
2022-08-04

At start-up, the display briefly shows the firmware version and model name on the boot splash screen. After 5 s, the display shows the number of active or total monitors (MONs Found) and sensors (Total Sensors) found, represented numerically. After an additional 5 s, if the fans are already configured, the display indicates Warming Up with a progress bar from left to right.

Note: If no fans are configured, the fan count is set to 0, and the host monitor prompts a completion of the Boot Fan Setup before warm-up. For more information, see Boot fan setup.