Front panel buttons - Johnson Controls - LIT-12014081 - RA-1270 - Airflow Measuring Station - AFMS

RA-1270 Advanced Thermal Dispersion Fan Inlet Airflow and Temperature Measuring System Technical Bulletin

Brand
Johnson Controls
Product name
AFMS
Document type
Technical Bulletin
Document number
LIT-12014081
Revision date
2022-08-04
Language
English

Use the five buttons on the front panel display, MENU, ESC, UP, DOWN, and ENTER to interface with the RA-1270 host monitor during system configuration setup and for certain functions in the normal operation mode. See Figure 1.