Configuration - Johnson Controls - LIT-12014081 - RA-1270 - Airflow Measuring Station - AFMS

RA-1270 Advanced Thermal Dispersion Fan Inlet Airflow and Temperature Measuring System Technical Bulletin

Brand
Johnson Controls
Product name
AFMS
Document type
Technical Bulletin
Document number
LIT-12014081
Revision date
2022-08-04
Language
English

The on-board microprocessor in the RA-1270 host monitor enables system configuration, operating parameter selection, analog output configuration, and display filtering. The host monitor also acts as a master across a wired network to up to 16 client monitor type controllers.

The operator or supervisor uses the RA-1270 configuration mode to verify configuration and change certain parameters within defined ranges. Use the five buttons on the RA-1270 host monitor front panel display cover to select configuration mode.