Factory default reset - Johnson Controls - LIT-12014081 - RA-1270 - Airflow Measuring Station - AFMS

RA-1270 Advanced Thermal Dispersion Fan Inlet Airflow and Temperature Measuring System Technical Bulletin

Brand
Johnson Controls
Product name
AFMS
Document type
Technical Bulletin
Document number
LIT-12014081
Revision date
2022-08-04
Language
English

Procedure

The Factory Default Reset sub-menu enables the user to reset all parameters back to the original default factory settings.

Note: If you perform a factory default reset, all configuration setup processes need to be performed. Operator and supervisor PINs, and any custom parameters are cleared. Selecting to clear fan data also clears the fan assignments, diameters, and field calibrations.

To perform a factory default reset, complete the following steps:

  1. While in the Supervisor Menu, use UP or DOWN to scroll to Factory Default and press ENTER.
  2. Use UP or DOWN to select Yes to confirm a reset to default settings. To also clear the fan assignments, diameters, and field calibrations, select Yes on Clear Fan Data? Otherwise those values are not reset.
  3. Press ENTER.
  4. The RA-1270 system automatically resets the settings of all sensors and devices to default, then performs a restart and warm-up. The RA-1270 then returns to the normal operational mode. All settings return to the default factory state.
  5. Use UP and DOWN to scroll through the possible connected devices on the monitor network to view the firmware version of each connected device.