OpenBlue Plant Optimizer security and network configuration considerations - Johnson Controls - LIT-12013045 - Software Application - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Security and IT Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document type
Security and IT Guide
Document number
LIT-12013045
Version
v2024.Q2
Revision date
2024-07-12

Plant Optimizer uses industry-standard system security and encoding protocols to protect against unauthorized access to data and control systems, and includes the following security features:

  • TLS 1.2/HTTPS and security certificates provide secure encrypted communication, which prevents unauthorized access.
  • The Plant Optimizer web application uses an automatically generated, self-signed CA Root certificate. If you want to use your own trusted security certificate, apply the customer certificate on your web server.

The Plant Optimizer server and client are located inside the site internal network, to ensure that the security considerations are the same as for the whole site.