Configure email notifications for changes to the operating mode, unavailable utility pricing, and unavailable monitored weather extend periods of adviser mode operation, and equipment being unavailable to Plant Optimizer, for example, due to manual overrides.
About this task
To set up Plant Optimizer with email notifications, contact CUP technical support and provide the following information:
- SMTP server name
- Required SMTP port Note: Indicate to technical support if you are not using a standard 25 SMTP port.
- Username and password credentials used to send the alert emails
Technical support enter the SMTP server name and credentials in the A3S agent app settings, as well as the email 'from' address in the form cpo-notifications@XXXX.com, where XXXX is the customer domain.
If you do not have SMTP credentials, use a Gmail® account.
To configure who receives each type of email notification, complete the following steps: