Working with the audit log - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04
The audit log continuously tracks user modifications to Plant Optimizer. When you make a modification to the operation of Plant Optimizer, you must enter an explanation. The audit log displays the following modifications:
  • Forecast input overrides
  • Manual input entries
  • Schedule changes
  • Mode changes
  • Plant model attribute changes
  • Admin changes

You can download the audit log as a .csv file. Use the Select Start Date and Select End Date to select the date range, and click Export to CSV.