Solver Performance dashboard - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04

You can use the Solver Performance Dashboard to view the algorithm execution performance. The line chart plots the time taken to execute the OpenBlue CUP algorithms solver. The Solver Performance Summary pie chart shows the percentage of solver executions in less than 1 minute, between 1 to 2 minutes, between 2 to 3 minutes, or more than 3 minutes, along with the total number of failed solver executions during the same user-specified period as the line chart.

About this task:
To generate the Solver Performance summary and line graph, complete the following steps:
  1. In the Administration interface, select Commissioning from the menu bar at the top of the page.
  2. In the Control Charts & Trends menu, select Solver Performance Dashboard.
  3. Specify the start date and end date for the time period of interest and click Generate Chart.

The line graph generates in the left pane and a chart of the Solver Performance Summary generates in the right pane.