Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04
About this task
Update the prediction model for a load
coil entity in the OpenBlue Plant Optimizer by pasting the prediction model byte array
text string generated in the OpenBlue Plant Simulator.
Procedure
In the Plant Optimizer administration application, from the menu
at the top of the page, select Commissioning.
Select Solver
Parameters, and search for all entities that include the LoadConsumed_Power/PredictorModel parameter.
Locate the relevant prediction model load coil entity in the
search results, paste the byte array string generated in the Plant Simulator,
and click Save to save the updated value.
To cancel an update, click Cancel Request.
Note: For persistent data associated with the byte array,
updates do not take effect until midnight. You can cancel a request before
this time. The audit log captures all manual requests and events.