Dispatch failures when required solver parameters are not mapped into Plant Optimizer - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04

Dispatches fail when the minimum required process variables and solver parameters are not mapped into Plant Optimizer. This means that points may need to be mapped, that were not previously mapped at the time of upgrading a site to the v2023.Q2 release.