About this task
To generate All Points Trends, complete the following steps:
Procedure
- In the Administration interface, from the menu bar at the top of the page, select Commissioning, in the Control Charts & Trends tab, select All Points Trends.
- From the Entity Name list, select the equipment.
- From the Point Urn list, select the data points.
- From the Data Source Name list, select the data source.
- Select a start date and end date.
-
Click Generate Chart.
Note: There is no limitation on the number of points that can be selected. However, the more points you select, the longer the plot loading time. There is a limitation on the chart tooltip (hover-over). If more than 10 points are selected, the tooltip may not show for more than 10 data points. Plots for periods longer than 14 days show hourly averages rather than raw data for each dispatch.You can use the Print and Download icons in the top right of the chart to print or download the generated chart. You can download the chart in PNG, JPEG, SVG, PDF, or CSV format.Note: When you download the CSV format, raw data is exported for the time period rather than hourly averages even if the period is longer than 14 days. If you select more than 10 data points, even though only up to 10 may display in the plot, the CSV file contains trend data for all of the selected data points.
- Optional: Click Add Chart to create an additional chart.