Working with the administration interface - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04

If you have administrator privileges, you can use the Administration interface to configure OpenBlue Plant Optimizer.

When you log on, from the pane in the center of the screen, select the Administration interface to configure the operation of the Plant Optimizer. The Administration interface contains the following sections:
  • User management
  • Configuration
  • Commissioning
  • Audit log
You can switch between administration mode and operator mode and do not have to log off and log on again.
Note: The switch functionality works only if you have administrator privileges.

To switch from administration mode to operator mode, click the drop-down list next to your profile name in top-right corner and select Switch to Operator. Click the drop-down list again and select Switch to Admin to switch back to administration mode.