Working with the monthly report - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04

The Monthly Report contains two types of report sections, Operating Mode and Monthly Savings. The Operating Mode report compares the time that the Plant Optimizer spends in each operating mode. The Monthly Savings report compares monthly average plant efficiency in kilowatt hours (kWh) to user-input baseline monthly average efficiency. The Monthly Savings feature is currently supported for electric chilled plants only.

In the navigation bar at the top of the page, click History and select Monthly Report from the menu.

For information about how to create the reports, see the following sections: