Deleting a schedule - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04

About this task

To delete a schedule, complete the following steps:

Procedure

  1. Select the schedule you want to delete.
  2. Click the Delete icon.
  3. In the You are deleting a repeating event window, you can delete Only this Event, delete All events, or Cancel the selection.
    • To delete the selected event only, click Only this event.
    • To delete all of the recurring events, click All.
    • To cancel the selection, click Cancel.
  4. If All is selected, the Delete Equipment Schedule window displays. In the window, the Add Reason for Deletion field is the only part that you can edit.
  5. Click Update.