Help - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OBEM Central Utility Plant Optimization - v2024.Q2

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Central Plant Optimization > OBEM Central Utility Plant Optimization
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2024.Q2
Revision date
2024-06-04

In the navigation bar, click the Help icon to access additional information and support for the Plant Optimizer.

User Manual in PDF
Click User Manual in PDF to view a PDF of the OpenBlue Plant Optimizer Administration and User Guide (LIT-12013036).
Interactive User Manual
Click Interactive User Manual to access the Johnson Controls Knowledge Exchange site and view the OpenBlue Plant Optimizer Administration and User Guide (LIT-12013036).
Note: This option is available only to users with an internet connection.
Video Tutorials
Click Video Tutorials to access OpenBlue Plant Optimizer training videos.
Contact Support
Click Contact Support to view the contact information for Plant Optimizer.
Suggest Enhancement
Click Suggest Enhancement to submit a product enhancement idea that you want to see in the Plant Optimizer application. For more information, see Submitting product enhancement requests.
Note: This option is available only to users with an internet connection.
L3 Support Files
Click L3 Support Files to download technical support files that you can share with Johnson Controls Level 3 (L3) Technical Support if a Level 2 support team cannot diagnose or resolve an issue in the Plant Optimizer application. For more information, see Downloading technical support files.
Note: Plant Optimizer websites that are airgapped cannot access any of the options other than the User Manual in PDF.