Adding ELDR overrides - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2024.Q1

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2024.Q1
Revision date
2024-03-20

Add or remove ELDR participation to include or exclude your system from the program on an hourly basis. To add an override, complete the following steps:

Procedure

  1. In the navigation bar at the top of the screen, click Response Program and select ELDR.
  2. On the left of the screen, click Add Overrides.
  3. With the Start Date & Time and End Date & Time options, configure the period of time that you want the override to operate.
  4. Select Participate or Do not participate to enable or disable participation in the ELDR program.
  5. Enter an explanation for adding an override. This explanation appears in the Audit Log. See Working with the audit log for further details.
  6. Click Save.

Results

The override appears in the ELDR Participation And Curtailment table at the bottom of the page. You can also click any available time period in the ELDR Participation And Curtailment table to add an override for that hour.