Working with the audit log - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2024.Q1

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2024.Q1
Revision date
2024-03-20
The audit log continuously tracks user modifications to Plant Optimizer. When you make a modification to the operation of Plant Optimizer, you must enter an explanation. The audit log displays the following modifications:
  • Forecast input overrides
  • Manual input entries
  • Schedule changes
  • Mode changes
  • Plant model attribute changes
  • Admin changes

You can download the audit log as a .csv file. Use the Select Start Date and Select End Date to select the date range, and click Export to CSV.