Creating users - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2024.Q1

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2024.Q1
Revision date
2024-03-20

Create users to enable and control access to CUP. To create a user, complete the following steps:

Procedure

  1. In the Administration interface, select User Management from the menu bar at the top of the page, and click Add User.
  2. In the First Name, Last Name, Username, and Email fields, enter the details for the user that you want to create.
    Note: The username must match the user domain name for domain authentication or the Metasys ADX username for local user authentication.
  3. From the Operational Roles list, select a suitable role that you want to associate with the new user. You can view the role permissions for each role in the list.
  4. From the Administration Roles list, select whether you want to associate the new user with administrative privileges. Only users with administrative privileges can view and edit the Administration interface.
  5. Optional: Select Add Another User if you want to add more than one user at a time.
  6. Click Create.