Model import - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2024.Q1

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2024.Q1
Revision date
2024-03-20

Use the Clobber Existing Parameters option to override existing solver parameters.

  1. In the Administration interface, select Commissioning, and select the Model Import tab.
  2. Under Clobber Existing Parameters, Off is selected by default. This means the values that are currently visible in the solver parameters can not change.
    Note: If you select On for the clobber solver parameters, an Attention message displays. Click Yes to confirm that you want to change the existing parameters as part of the model deploy.
  3. Click Find Model to import a model with the updated values.
  4. Click Upload.
  5. In the Confirm Model Import window, enter your user name and password. Click Reauthenticate.

After you import the model, the values are updated in the Solver Parameters tab.