Generating control charts - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2024.Q1

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2024.Q1
Revision date
2024-03-20

About this task

To generate Control Charts, complete the following steps:

Procedure

  1. In the Administration interface, from the menu bar at the top of the page, select Commissioning, in the Control Charts & Trends tab, select Control Charts.
  2. From the Entities list, select the equipment.
  3. From the Points list, select the data points.
  4. From the Datasource list, select the data source.
  5. Select a start date and end date for the generated control chart.
  6. Click Generate Chart.

    You can use the Print and Download icons in the top right of the chart to print or download the generated chart. You can download the chart in PNG, JPEG, SVG, PDF, or CSV format.

  7. Optional: You can generate multiple charts for different data points as you require. Click Add Chart to create an additional chart.