Creating a monthly savings report - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2024.Q1

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2024.Q1
Revision date
2024-03-20

Create a simplified monthly savings tracker report to review actual monthly average plant efficiency in kilowatt hours (kWh) compared to user-input baseline monthly average efficiency. You can generate a report for the entire site or a single plant, but the entire system must be electric chilled water plants. The savings values in the report are not the actual savings, but rather a proxy metric for directional representation of savings.

Procedure

  1. In the navigation bar at the top of the page, click History and select Monthly Savings from the menu.
  2. In the Monthly Savings pane, from the Compare list, select what you want to compare.
  3. From the Subplant list, select a subplant.
  4. From the Start Date and End Date calendars, select a start date and an end date for the report.
  5. Click Generate Chart.

    Use the Reset Zoom, Print, and Download icons in the top right of the chart to reset the zoom, print, or download the generated chart. You can download the chart in PNG, JPEG, SVG, PDF, or CSV format.

  6. Optional: Click Add Chart to create additional monthly savings reports.

Results

The monthly savings report displays. A simplified representation of savings for the month to date and the year to date also display in the top-right of the report.