Solver parameters - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

Use the solver parameters to search for and add entries that can be used in the model-based optimization, such as design parameters, performance model coefficients, constraints, or optimization settings.

Select from the following two views to make solver parameter changes:
  • Data schema: You can search the parameters by schema (parameter name, parameter class template, model entity name) and edit the entries one by one. Any changes you make in this view is reflected in the equipment type view.
  • Equipment type: You can compare or update multiple entries of the same type of equipment at the same time. Any changes made in this view are reflected in the data schema view.