Dispatch failures when required solver parameters are not mapped into Plant Optimizer - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

Dispatches fail when the minimum required process variables and solver parameters are not mapped into Plant Optimizer. This means that points may need to be mapped, that were not previously mapped at the time of upgrading a site to the v2023.Q2 release.