Working with the administration interface - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product name
OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

If you have administrator privileges, you can use the Administration interface to configure OpenBlue Plant Optimizer.

When you log on, from the pane in the center of the screen, select the Administration interface to configure the operation of the Plant Optimizer. The Administration interface contains the following sections:
  • User management
  • Configuration
  • Commissioning
  • Audit log
You can switch between administration mode and operator mode and do not have to log off and log on again.
Note: The switch functionality works only if you have administrator privileges.

To switch from administration mode to operator mode, click the drop-down list next to your profile name in top-right corner and select Switch to Operator. Click the drop-down list again and select Switch to Admin to switch back to administration mode.