Creating an operating mode report - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

Use the Monthly Operating Mode Report to compare the time that the Plant Optimizer spends in each operating mode. The report displays a percentage of the time spent in each mode for each month in a specified time period.

About this task

To create an operating mode report, complete the following steps:

Procedure

  1. In the navigation bar at the top of the page, click History and select Monthly Report from the menu.
  2. In the Operating Mode pane, from the Start Date and End Date calendars, select a start date and an end date.
  3. Click Generate Chart.
  4. Optional: Click the Download icon on the right-side of the chart to download the chart.
    Note: There are four modes that can be displayed on the chart, Unavailable, Advisory, Auto, and Missing Data. Missing data is where the dispatches fail or the dispatches are not available for the selected time frame.