Working with the monthly report - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

The Monthly Report contains two types of report sections, Operating Mode and Monthly Savings. The Operating Mode report compares the time that the Plant Optimizer spends in each operating mode. The Monthly Savings report compares monthly average plant efficiency in kilowatt hours (kWh) to user-input baseline monthly average efficiency. The Monthly Savings feature is currently supported for electric chilled plants only.

In the navigation bar at the top of the page, click History and select Monthly Report from the menu.

For information about how to create the reports, see the following sections: