Creating a scatter chart - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

Procedure

  1. In the navigation bar at the top of the page, click History and from the list, select Scatter Charts.
  2. From the Plant list, choose the plants you want to compare. Plants are organized by loop.
  3. From the Chart Type list, select Single Time Period, Compare by Operating Mode, or Compare by Time Period. The Compare by Operating Mode option displays patterns of differences in plant efficiency between Plant Optimizer running in Auto mode versus Advisory mode.
  4. A start date and an end date for the report are selected by default. Use the Start Date and End Date calenders to change the preselected dates.
    Note: If an overlap exists in the start and end date range, you are notified with an error message.
  5. Click Generate Chart.