Modifying a recurrence schedule - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product name
OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

After you add a recurring event schedule, you can now edit or delete the occurrences individually and collectively.

About this task

To modify a schedule, complete the following steps:

Procedure

  1. Select the schedule you want to change.
  2. Click the Edit icon to modify the recurrence schedule.
  3. In the You are changing a repeating event window, you can edit Only this Event, edit All events, or Cancel the selection.
    • To edit only the selected event, click Only this event.
    • To edit all of the recurring events, click All.
    • To cancel the selection, click Cancel.
  4. If All is selected, the Edit Out of Services Schedule window displays. In the window, you can choose the Type of Schedule, the Duration of the Schedule and edit the Start Time and End Time and the days of the schedule.
  5. Click Update.