Importing a campus schedule - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

With the Plant Optimizer, you can import a Metasys campus schedule , as an XML file, to plan for holidays and out-of-session periods from that schedule. An imported schedule updates only future data and any existing future data is overwritten. Past data is not affected when you import a schedule.

Procedure

  1. In the navigation bar at the top of the page, click Future Inputs and select Campus Schedule on the right side of the drop-down menu.
  2. In the upper left of the page, click Import Campus Schedule.
  3. In the Import Equipment Schedule window, in the Schedule Name field, enter a name.
  4. Click Find Schedule, and upload the appropriate schedule.
  5. Enter a comment, and click Import.