Working with forecast inputs - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

Use the Forecast Input Summary page to obtain an overview of the data values that the Plant Optimizer predicts, and the data values that the Plant Optimizer ingests from third parties.

  1. To view the Forecast Input Summary page, in the navigation bar at the top of the page, click Future Inputs and select Summary on the left of the drop-down menu.
  2. Hover over the chart to view hourly data point information. The red line represents the current time, and yellow shading on the chart indicates an active forecast override. For more information about overriding forecast inputs, see Overriding a forecast input.
  3. Click a forecast input name to view the forecast input detail page for an input.