Getting started - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q4

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2023.Q4
Revision date
2023-12-01

Before you log on, work with your site administrator to identify the domain, user name, and password combination that you can use to access the system. The following two different interface options are available in Plant Optimizer:

  • Administration: Use the administration user interface to create and configure user accounts, user permissions, and configure your site. For more information, see Working with the administration interface. If you have administrative privileges and you want to configure the operation of the Plant Optimizer, when you log on, select Administration from the pane in the center of the screen. Otherwise, to monitor and control Plant Optimizer, select the operational user interface Operate.
  • Operate: Use the operate user interface to monitor and control your system. If you are assigned to an operator role, you do not need to select this role and you automatically log on as an operator.