Adding a fault rule to the maintenance adviser - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q3

OpenBlue Plant Optimizer Administration and User Guide

Brand
Johnson Controls
Product name
OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q3
Revision date
2023-09-05
Language
English

To add a new fault rule to the maintenance adviser, complete the following steps:

Procedure

  1. In the Plant Optimizer administration application, from the menu at the top of the page, select Configuration and Maintenance.
  2. Select Add Fault Rule and enter the details of the fault rule. When you select the Health Check and system type, the related equipment selection is automatically populated. Next, select an equipment variable for the fault rule, and set the equipment tolerance. The tolerance value is automatically set with a default value based on the health check type.