Generating all points trends - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q3

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2023.Q3
Revision date
2023-09-05

About this task

To generate All Points Trends, complete the following steps:

Procedure

  1. In the Administration interface, from the menu bar at the top of the page, select Commissioning, in the Control Charts & Trends tab, select All Points Trends.
  2. From the Entity Name list, select the equipment.
  3. From the Point Urn list, select the data points.
  4. From the Data Source Name list, select the data source.
  5. Select a start date and end date.
  6. Click Generate Chart.
    Note: You can plot only four points at a time. Plots for periods longer than seven days show hourly averages rather than raw data for each dispatch.

    You can use the Print and Download icons in the top right of the chart to print or download the generated chart. You can download the chart in PNG, JPEG, SVG, PDF, or CSV format.

  7. Optional: Click Add Chart to create an additional chart.