You can make the Plant Optimizer aware that plant operations are suspended in the future with the Plant Disable Schedule feature. This marks a defined period of time as a period where the normal schedule does not apply. The yearly schedule and the daily schedule are the two options, which you can use to add a plant disable schedule. The yearly schedule is used for defining seasonal periods where either the plant is off or during periods where a daily shutdown schedule applies. This functionality is available at daily, weekly, and monthly levels.
About this task
To access the Plant Disable Schedule, complete the following steps: