Weather prediction for air-gapped sites - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q3

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q3
Revision date
2023-09-05
Plant Optimizer can provide future weather predictions, particularly for short-term forecasts (1 hour to 4 hours ahead), in the following cases:
  • If a site cannot connect to standard weather forecasting services that Plant Optimizer uses, such as AccuWeather or U.S. National Oceanic and Atmospheric Administration (NOAA) National Weather Service, over the Internet due to cybersecurity policies.
  • If local plant automation systems have data points available for local on-site weather stations or outdoor air ambient condition sensors mapped that can be integrated.
Installation Note:
When you upgrade a Plant Optimizer site that receives weather forecasts from Accuweather or NOAA to v2023.Q2 from a prior release, you must configure the following Solver Parameters as False for dispatches to pass:
  • Weather/Drybulb/EnablePrediction
  • Weather/Wetbulb/EnablePrediction
  • Weather/CloudCover/EnablePrediction
  • Weather/EarthWaterTemperature/EnablePrediction
  • Weather/EarthWaterTemperatureAlternate/EnablePrediction

You should configure these parameters as True for predictors with on-site weather measurements mapped to the actual value and have a predictor byte array defined and enabled in Solver Parameters, typically for air-gapped sites. A site may have some weather that is mapped and some weather that is not mapped.