Uploading a mass prediction override file - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q3

OpenBlue Plant Optimizer Administration and User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Central Utility Plant
Document number
LIT-12013036
Version
v2023.Q3
Revision date
2023-09-05

Apply the mass prediction override to the override imported weather forecasts or campus load predictions. To upload a mass prediction override file, complete the following steps:

Procedure

  1. In the navigation bar, click Future Inputs.
  2. Select Campus Loads or Weather and click Override.
  3. In the override window, enter the required information.
  4. In the Change field, select Upload Loads (CSV) from the list.
  5. Click Download Template, and input the appropriate data into the .CSV file template.
  6. Click Browse and upload the appropriate file.
  7. Click Save.