Enabling email notifications for the Plant Optimizer - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q1

OpenBlue Plant Optimizer Administration and User Guide

Brand
Johnson Controls
Product name
OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q1
Revision date
2023-02-28
Language
English

To set up the Plant Optimizer with email notifications, contact Johnson Controls technical support and provide the following options:

  • SMTP server name
  • Required SMTP port
  • User name and password credentials used to send the alert emails

The SMTP server name and credentials are entered by CUP technical support in the Optimizer configuration file, along with the email 'from' address in the form cpo-notifications@XXXX.com, where XXXX is the customer domain.

If SMTP credentials are not provided, a CUP Gmail account is used instead.