Deleting a schedule - Johnson Controls - LIT-12013036 - OpenBlue Central Utility Plant - OpenBlue Central Utility Plant - v2023.Q1

OpenBlue Plant Optimizer Administration and User Guide

Brand
Johnson Controls
Product name
OpenBlue Central Utility Plant
Document type
Administration Guide
User Guide
Document number
LIT-12013036
Version
v2023.Q1
Revision date
2023-02-28
Language
English

About this task

To delete a schedule, complete the following steps:

Procedure

  1. Select the schedule you want to delete.
  2. Click the Delete icon.
  3. In the You are deleting a repeating event window, you can delete Only this Event, delete All events or Cancel the selection.
    • To delete only the selected event only, click Only this event.
    • To delete all of the recurring events, click All.
    • To cancel the selection, click Cancel.
  4. If All is selected, the Delete Equipment Schedule window displays. In the window, the Add Reason for Deletion field is the only part that can be edited.
  5. Click Update.