Configure transceivers with the following credentials:
- The relevant wireless network Wi-Fi SSID details.
- The associated security key that connects to the Wi-Fi network.
Location Manager transceivers require the following conditions for Wi-Fi connectivity:
- For transceivers to access Bluzone Cloud, the wireless network must allow automated and non-expiring login.
- Wi-Fi is machine to machine optimized and does not implement HTML sign-on.
- The only compatible certificate formats are .pem and .der.
- Transceivers are compatible with 2.4GHz band Wi-Fi only.
- Transceivers support an 802.11 b/g/n network.
- Networks that support a large number of transceivers and beacons, for example, 800 beacons or 200 transceivers, require an upload speed of at least 8 Mbps.
- Enable MAC address filtering. Add the MAC of the transceiver to the whitelist.
- Ensure that the HTML5 web socket traffic is not blocked.
Configure these ports to support transceiver connectivity:
- 443: The transceiver uses an https and WSS web socket connection to communicate with the cloud application.
- 123: The transceiver uses this port to connect with NTP (Network Time Protocol) information.