New features - Johnson Controls - LIT-12013859 - OpenBlue Location Manager - 2.5.8

OpenBlue Location Manager Release Notes

Brand
Johnson Controls
Product name
OpenBlue Location Manager
Document type
Release Notes
Document number
LIT-12013859
Version
2.5.8
Revision date
2023-06-16
Language
English

OpenBlue Location Manager now contains the following feature enhancements:

  • Add and edit a time schedule to turn devices on and off

    Admins can now set a time schedule to turn equipment on and off directly from the Configuration UI if the equipment is connected to a Moko device. This feature allows you to set a time schedule for each piece of equipment that automatically turns on and off based on your needs. This feature makes it easy to achieve energy savings by turning off the equipment automatically when it is not needed, such as nights and weekends.

  • New Equipment Recommendations dashboard

    Users can now avail of a new Equipment Recommendations dashboard that gives equipment utilization insights. From this dashboard users can now see a list of recommended actions regarding low battery levels on badges and offline transceivers.